Too often in our industry today, we see a manufacturer's commitment to the end-customer measured exclusively in the length of the warranties offered. At Belden, we have a significantly different approach.
We believe the best warranty program is the one our customers never have to use, and throughout our history of providing quality products, service and support, that has routinely been the case. Still, because Belden has a lifelong commitment to standing behind our products, our customers get one of the most comprehensive warranty assurance programs in the industry.
- IBDN 25-Year Product Warranty
For end-to-end copper and optical fiber systems, Belden offers the strongest certification program in the industry. In effect from the date of installation, our 25-Year Product Warranty warrants against defects in materials and workmanship. For the same period, these components are guaranteed to meet or exceed the specifications of standards organizations including ISO/IEC, CENELEC and TIA/EIA for the category of Belden IBDN System installed. - IBDN Lifetime Application Assurance Program
Belden warrants that the IBDN Certified System will be capable of operating the applications, which the System was originally designed to support, as well as any new applications, for as long as you own the System in its original place of installation. New applications are defined as any application introduced in the future by recognized standard organizations or user forums that use the TIA/EIA-568-A or ISO/IEC IS 11801 component and link/channel specifications for cabling. Also guaranteed are the Systems' specified throughput rate and minimum bandwidth capabilities. - Performance & Warranties Profile for Belden:
IBDN 10GX System Installations
IBDN 4800LX Certified System Installations
IBDN System 3600 Certified System Installations
IBDN System 2400 Certified System Installations
IBDN System 1200 Certified System Installations
IBDNPlus Category 5 Certified System Installations
IBDN FiberExpress System Installations
- Belden's Trapeze Networks Wireless Solution
For the Trapeze Network Wireless Solution, Belden offers a 12-month warranty with a return and replacement policy. This is backed by a 90-day software support program that provides for free software upgrades and phone, online and email support during the warranty period. Thereafter, customers may purchase extended warranty programs ranging from software-only support to advanced hardware replacement. No other company offers such a high quality product line- backed by the industry's strongest support organization and its warranties. You can always depend on Belden to exceed your expectations. - 10-Year Belden Product Warranty
All A/V, building management, and security installations come with Belden's exclusive 10-Year product warranty. This warranty provides the enterprise customer with comprehensive coverage against defects in materials and workmanship.
Always Just a Phone Call Away
At Belden, we've taken every step to ensure the highest quality products, optimal system performance, simplified building operations, best design and installation and warranty assurance. But we also believe no question should ever go unanswered, which is why we're always just a phone call away.
Call 1.800.BELDEN.1 anytime for more information about our products and partners, or to learn how Belden Total Enterprise Networks can fulfill your unique Enterprise application needs.