Industrial Security
Industrial Ethernet
Data Centers
Broadcast AV
Belden News
Blog Home

The Strange World of Cat 5e and Cat 6

Posted by: Steve Lampen on October 08, 2013

I remember at Belden when we started to work on a new data cable around 1993-94. Its secret "in-house" name was DATA-X. This was during the four years in lived in Richmond, Indiana, the location of Belden's biggest factory. (Our corporate offices have since moved to St. Louis.) When I saw the test data for "DATA-X" I got very excited. Clearly this was a breakthrough cable. So much so that I realized it had potential to carry lots of other signals besides just 10BaseT or 100BaseT Ethernet. So I begged our marketing folks NOT to use the word "data" in the name of the product. (The previous product was DataTwist 350.) If it was called DataTwist all people would use it for was data. Instead, I came up with the name MediaTwist. (One other Belden sales guy, Mike Masucci, will argue with me on this. He says HE came up with the name.)

Whoever it was, this was the right call! This stuff (Belden 1872A - riser- and Belden 1874A - plenum) blew away other cables, and still does in many ways almost twenty years later. I started to talk in public about using this kind of unshielded twisted pair (UTP) cable to run non-data applications such as analog and digital audio. At first, I saw lots of heads going back and fourth ("No!") in my audience. But now, running audio on Category 5e or better is old news and many are doing it. The first real breakthrough for me was Dr. Fred Bashour, who recorded classical music in the field. I sent him some MediaTwist. He was amazed, and never looked back.

Now I could start to tell you WHY it is so great, so low in noise pick-up, so rugged, how it eliminates ground loops (well, it doesn't have a shield or drain wire). But forget all that. Below is a picture of Watson Wu. He specializes in film sound and sound effects. Here he is recording in the field. You will note the shotgun shells on his vest and the ammunition and serious weaponry on the table. We're talking real dynamic range here!

B60_Watson Wu - InstaSnakes - TOS_1588

(Pictures are courtesy of Watson Wu)

In between all those microphone cables behind him are strange little boxes. Here they are close up:

B60_InstaSnakes - TOS_1624

(Pictures are courtesy of Watson Wu)


You'll notice that for every four microphone cables, there is a fifth cable in the middle. And what is that cable? A Category 5e or 6 cable! Those four microphone signals are carried by the four pairs inside the data cables. These little boxes are called InstaSnake and made by a company called ETS in Fremont, California. (www.etslan.com). These are clever boxes. If you hook them up with UTP, unshielded twisted pair Category 5e or 6, they work just fine but there is no ground connection. For self-powered or dynamic microphones this is just fine. Of course, the noise rejection comes from the fact these are twisted pairs that are differentially-driven balanced lines, with the best balance (CMRR) ever created in a twisted pair. And the best data cable for rejecting noise, among all the data cables, is the one with the "deepest" CMRR. That would be one of our Bonded-Pair cables such as Belden 1700A (DataTwist 350) or Belden 1872A (MediaTwist). There are many more Belden Bonded-Pair cables than just those, you can find them at www.belden.com.

The real breakthrough for the InstaSnake was the first Obama Inauguration. These boxes were all over the place and a lot of the audio you heard that day was going through Category 5e or Cat 6 cables. And, in a pinch, you can use the same Category 5e or 6 cable to run data! (That's a joke.) So, if you're an audio designer or installer, consider data cable for your next "problem install", especially the Belden Bonded-Pair varieties. What this stuff can do might just amaze you. No shield, no drain wire, no ground means no ground loops, a major source of noise and interference in audio. And since we're using Bonded-Pairs, that can't separate and move around, they are almost immune to impact noise ("triboelectric" noise or capacitive noise) which can be a problem for cables in the fields being walked on or rolled over.

If you have phantom-powered condenser microphones, then you have to have a ground. It's part of the delivery system of phantom power. So just change to a shielded Category 5e such as Belden 1212F or shielded Category 6 such as Belden 2412F.The RJ-45 connector on the InstaSnake is also shielded, and these shields are connected to all the "Pin 1's" in each XLR. Of course, then you are back in "ground loop" territory, so be careful about the grounds at each end of your run. They need to be at the same potential to be effective at noise reduction. ETS also makes a version of InstaSnake which sacrifices one pair out of the four inside a Category 5e or UTP as the ground connection. No shield then, just a ground connection for phantom power and other systems that absolutely require a ground connection to work. You get three channels of audio plus one pair as a ground. So, surprisingly, you could still use our UTP cables for phantom power.

If you look closely at the photo, you will see these are not just garden-variety RJ-45 connections on the InstaSnake, but Neutrik "Ethercon". That means you can use a rugged data cable, such as Belden 1305A (Category 5e). Again, Bonded-Pairs, but with a double jacket. The inner jacket connects to the RJ-45, the outer jacket to the Ethercon shell, so any strain on the outside of the cable is not transferred to the inside. Pretty neat! There's even a cloth layer between the two jackets to make SURE they slide. It is so flexible, you would swear it is microphone cable. Flexible and rugged are very rare to see in the same cable. Belden 1305A is still UTP (unshielded) and lots of people worry about the crosstalk between pairs, especially at mic level (-50 dBm, -60 dBm). In fact, a really bad data cable consistently shows -100 dB of noise or crosstalk rejection at audio frequencies. For a cable like MediaTwist, we CAN'T READ the crosstalk rejection on our $60,000 Agilent (H-P) network analyzers. It's below the analyzer noise floor (-110 dB) at audio frequencies!

Belden also makes lots of super-heavy-duty Industrial Ethernet cables, such as Belden 7921A. It's Category 5e DataTuff with a foil and braid shield and is intended for Factory Floor Ethernet. So it might be harder to find. Our audio-video distributors are unlikely to carry it, since it is in our Industrial line. It's very big. I'm not even sure it would fit into a Neutrik Ethercon, but there are many factory-rugged RJ-45 connectors made for it. Using it in a field recording situation, like we're talking about, is pretty much like using a Sherman Tank to go to the supermarket. But I'm sure there are times you wished you had a Sherman Tank at the supermarket! (You would ALWAYS find a parking space, and right where you wanted one.)

You can go check out the details on any of these cables at www.belden.com. Just click on "products" and choose the eCatalog below. Put in the part number and hit the arrow. Click on the picture of the cable you want when it shows up. The background turns blue,and then choose "Tech Data" above it. You will then get every gory detail about that cable or any cable we make. Want a sample? Call our Customer Service Department 1-800-235-3361 (1-800-BELDEN-1). They'll send you a short sample of any of these cables. Want a longer one to test? Then you need to talk to me. Just send me an email steve.lampen@belden.com or just fill in the Comment Box below. Thanks for reading!

Tags:Data

Bookmark and Share

Comments

 
  1. Harry Hale
    April 27, 2016 at 06:02
     

    Thank you good info. noise rejection specs do not surprise me after all Bell (ATT) ran useful audio over thousands of miles of twisted pair in the old days. 30 years ago I did a basket ball game that CBS broadcast I was the Arena sound man. CBS had Mountain Bell run dry phone lines where ever they wanted to such as the arena sound booth for remotes. They had little adapters binding post to XLR.

     
  2. Steve Lampen
    July 10, 2014 at 09:14
     

    Riki- Cat 5 (which is no longer part of the standard) and Cat 5e (which replaced it) are both 100 MHz bandwidth. Cat 6 is 250 MHz bandwidth. This is just the tip of these icebergs. The entire specification for each is different. Crosstalk number (both near-end and far-end) are tighter in Cat 6 than in Cat 5e. Attenuation, return loss and many other specification are also tighter, hard to get to, in Cat 6 than Cat 5e. For a synopsis from the cable side, e-mail me at steve.lampen@belden.com and I will send you the TIA Standards Spec Comparison.

     
  3. July 02, 2014 at 06:56
     

    What is diffence between the cat-5 and cat-6? Anyone explain it..

     
  4. October 15, 2013 at 05:38
     

    Steve, Wonderful article chock-filled with good facts to know. Thanks! Trudy

     
 

Post A Comment






 
Follow Us

Subscribe
Broadcast AV
RSS Feed
Broadcast AV
Email Notifications

Search
Broadcast AV Blog
All Belden Blogs


Stay Informed