Industrial Security
Industrial Ethernet
Data Centers
Broadcast AV
Belden News
Blog Home
Blog Category: Industrial Ethernet

Posted by: Ryan Rouse on May 17, 2017

The oil and gas industry is poised for growth this year. But, key to the sector’s success will be overcoming new challenges, such as cyber security threats, regulatory changes and increased safety concerns, all while keeping operational costs down.

Core to this success is communication continuity, which can be achieved by investing in a solid and reliable network infrastructure that delivers superior performance, even in harsh and dynamic environments. Is your company equipped with the right resources? Click “Read More” below to learn more.

Read More >>


Comments (0) Post a Comment

Blog Category: Industrial Ethernet

Posted by: on January 14, 2015

In order to enhance the reliability and availability of data communication in hazardous operations areas, many are shifting to industrial Ethernet-based network designs.

You may think that Ethernet devices are suitable for control room use only. New technology, however, now enables network managers to place them in operations areas, even those under vibration strain or excessive heat.

In this blog, we will look at four key considerations when selecting networking products for an operations area: installation needs, industry approvals, environmental conditions and timing. A downloadable Application Note is also available, which details how this approach was applied to Belden’s recent work with a major European ship engine producer.

Read More >>


Comments (0) Post a Comment

Blog Category: Industrial Ethernet

Posted by: on August 20, 2014

Many businesses in industrial settings – including food and beverage, energy, manufacturing, pharmaceutical and more – are feeling pressure to trim costs and improve margins. As a result, we’ve seen an explosion in connected systems that automate processes and increase productivity. While these systems have been a boon for many businesses, the extreme and hazardous conditions of many industrial environments present significant new challenges for reliability and maintenance.

The high-intensity shock and vibrations, extreme temperatures and powerful chemical agents of many industrial settings can wreak havoc on the cord sets and cabling components used to enable connected, automated systems – leading to increased maintenance costs, or worse, unplanned downtime.

That’s where wash-down cord sets – an emerging category of ruggedized cables and connectors – can help. Wash-down cord sets are designed to withstand the harshest industrial conditions, helping to protect against unplanned system downtime while driving down maintenance and repair costs.

Read More >>


Comments (0) Post a Comment

Follow Us

Subscribe
Industrial Ethernet
RSS Feed
Industrial Ethernet
Email Notifications

Search
Industrial Ethernet Blog
All Belden Blogs


Stay Informed