Technical Papers


How Wire Fails
Originally presented to the Society of Motion Picture and Television Engineers Convention,
Sydney, Australia, on Friday, July 4, 1997.

By Stephen H. Lampen
Technology Development Manager
Belden

ABSTRACT:

Wire and cable can fail from a number of causes. This paper is an overview of the various failure modes wire can exhibit, how to predict each and how to help prevent it. Often, installers or users mistakenly suspect one failure mode when in fact another (or even none) is to blame. This article will also present an analysis template to determine just which failure mode might be expected.

ACRONYMS:

PE: polyethylene
PP: polypropylene
PVC: polyvinyl chloride
SRL: structural return loss

FAILURE MODES:

Wire and cable can fail in a number of ways. These include:

INSTALLATION FAILURE: The wire or cable was not installed correctly, or not installed to correct installation practices or industry standards. This can often involve poor connector choice or incorrect connector installation.

ENVIRONMENTAL FAILURE: The wire or cable is not intended for the place it is installed. This may involve outdoor, direct-burial or other ruggedness requirements, or cable installed in electronically "noisy" areas without adequate protection, or in high or low-temperature applications where the cable is not manufactured for such environments.

OPERATIONAL FAILURE: The inherent limitations of the wire or cable were not understood by the designer, purchaser or installer. The cable can be run too far or a poorly-manufactured version may be substituted for one of higher quality. This is commonly known as the "just as good" syndrome.

MANUFACTURING FAILURE: The wire or cable was incorrectly manufactured, incorrectly labeled, or incorrectly tested. Cable could be made on machinery out of tolerance, in need of maintenance, or not designed for the precision required in many current designs. This can include substandard or flawed product being sold as "normal" product. Cable failures of this kind may or may not be apparent to the designer, purchaser or installer.

 

INSTALLATION FAILURE:

Installation failure can be caused by the wire or cable not being installed correctly, or not installed to correct installation practices or industry standards. This can often involve poor connector choice or incorrect connector installation.

General Installation Guidelines:

Here is a chart of standard practices for audio and video cable:

Type of Cable Specification Standard Practice Comments
microphone reliability cable preparation combing out braid/sleeving
soldered pins insulation displacement ?
line-level analog audio bend radius > 4 times diameter not critical
pull strength each cable different consult manufacturer
digital audio bend radius > 4 times diameter affects impedance
pull strength each cable different consult manufacturer
baseband video bend radius > 10 times diameter solid vs foam
pull strength each cable different consult manufacturer
connector choice analog 50OHMS10.gif (838 bytes) or 75OHMS10.gif (838 bytes)
digital video bend radius > 10 times diameter gas-injected foam
pull strength each cable different consult manufacturer

connector choice

digital 270 Mbps

single runs: 50ohms10.gif (838 bytes) or 75ohms10.gif (838 bytes)

multiple connectors in line: 75ohms10.gif (838 bytes)

broadband video reliability installer quality? F connector standard
pull strength long runs/aerial messengered
performance DBS = 1.8 GHz high velocity foam

 

Conduit Issues

Question

Reason

Answer

Comments

How many cables will be pulled through each conduit? Only so much room. In the states, the standard is 40% fill. Pull force requirements go up exponentially after 40 %
How straight a run is it? The straighter the run, the easier the pull. MAXIMUM of two 90 bends in one pull. Combine angles for max. of 180
Correct cable choice? Some cables pull easier than others Stiff cables with shiny jackets pull better than flexible cables with matte jackets. Conduit is the best shield of all. Why buy fancy super-flexible cables with braid or serve shields just to install them in conduit?
Has the architect changed the size of the conduit in a cost-cutting measure? It happens! Did you change the cable pulls to follow the change in diameter? A change from one size to the next size down will almost guarantee you will exceed conduit fill and maximum pull strength.
Pulling tools and methods Makes life easier! Snake/fish tape, pulling compounds, pulling basket Maybe non-conduit cable isn't so expensive after all!

 

How to Determine Conduit Fill:

Determine area of conduit. Figure internal diameter, not external. Manufacturer of cable should provide circular area for each cable. You can then simply add the cable areas until you reach 40% of conduit area.

ENVIRONMENTAL FAILURE:

Environmental failure means the wire or cable is not intended for the place it is installed. This may involve outdoor, direct-burial or other ruggedness requirements, or cable installed in electronically "noisy" areas without adequate protection, or in high or low-temperature applications where the cable is not manufactured for such environments.

Construction Special Difference Jacket

Comment

Outdoor Crush-resistant internal components Gel-filled to avoid water penetration High-density black PE No fire-rating
Noisy area w/ audio analog braid high braid coverage PVC Below 10 MHz
digital foil folded foil PVC Wide bandwidth
Noisy area w/ video analog double braid high braid coverage PVC 6 MHz
digital foil/braid high braid coverage PVC <135 MHz

 

OPERATIONAL FAILURE:

Operational failure is caused by inherent limitations of the wire or cable which were not understood by the designer, purchaser or installer. The cable can be run too far or a poorly-manufactured version may be substituted for one of higher quality. This is commonly known as the "just as good" syndrome.

Here's how to determine the construction and performance quality of various audio cables:

Center Insulation Shield Jacket
Good copper PVC Serve/spiral PVC
Better copper PP Foil PVC
Best copper PE Braid
French Braid
PVC
PE
Rubber
Notes purity?? Pick by capacitance Foil for RFI
Braid for DC to 10 MHz
High-density PE for outdoor/UV resistance.

While there are no "standards" for analog audio, with a very low frequency range (20 Hz to 20 KHz), the wavelengths are so long that the impedance of the cable itself is of no consequence. What does affect performance is capacitance, resistance, and shield effectiveness. Flexibility, flex-life and ruggedness may also be a consideration.

Here's a chart to determine the quality of baseband video cable:

Center Conductor Dielectric Shield Jacket Comments
Analog solid copper solid PE (best) double braid PE (fire?) 6 MHz bandwidth
foam PE (good) braid PVC
Digital solid copper foam PE foil/braid PVC <135 MHz
Notes no copper-clad steel NO PVC bandwidth? HDTV coming

Here's a chart to determine the quality of broadband (CATV) video cable:

Conductor Dielectric Shield Jacket Frequency
Analog copper-clad steel
50 MHz and above
foam PE foil/braid PVC if indoor only 1 GHz
Digital copper-clad steel
50 MHz and above
foam PE foil/braid PVC if indoor only DBS =
1.8 GHz
Notes 30-50 MHz interactive? foam velocity >80% braid not critical High-density black PE if outdoor

MANUFACTURING FAILURE:

Manufacturing failure means the wire or cable was incorrectly manufactured, incorrectly labeled, or incorrectly tested. This can include substandard or flawed product being sold as "normal" product. Manufacturers may also be using old machinery, machinery in need of maintenance or which is otherwise out of adjustment. Manufacturers may also be using older machinery not designed to produced cutting-edge technology products. Cable failures of this kind may or may not be apparent to the designer, purchaser or installer.

Periodicity:

If you can get a graph instead of just a number on the structural return loss (SRL) on a cable, this can tell you a lot. Because of the complexity, most manufacturers only test an occasional roll of cable. SRL will tell you about changes in capacitance, impedance, conductor size, cable dimensions and, most insidious of all, periodicity.

Periodicity is the accumulated errors built up because of periodic flaws in the cable. For instance, say you have a wheel in your extruder which is out of round. This may stretch the center conductor making it microscopically thinner at one point. Or the dielectric might come out slightly smaller in diameter for each turn of the wheel. While such a change is very minor, and may not even be readable with test gear, or noticeable in use, this flaw will be added over and over and over again each time the wheel turns.

This now adds the dimension of multiple flaws at the same spacing. If you have a flaw every 100 cm, over and over, this distance corresponds to a wavelength of a specific frequency. While a 100 cm flaw creates a major flaw at 3 GHz fundamental frequency, this anomaly will also show up to a lesser extent at every harmonic of 3 GHz. It doesn't take many divisions to get to key frequencies for cable television, digital video, digital audio and similar applications. Also, this problem would not be a factor if the cable were cut short, perhaps 10 meters or less. But, with increasing distance, this minor flaw could be a major cause of SRL. Drop-outs of whole channels in CATV cable, or loss of critical data in digital video, could result. And there is nothing in the manufacturers catalog to tell you. You can't even tell by looking at the cable.

Compound migration.

If cables are used outdoors, or in harsh environments, the chemicals that make up the jacket are critical. If they are low quality materials, they can leach or "migrate" into the dielectric. This is another good reason for a foil as part of the shield. Foil helps prevent this.

If the chemical constituents of the jacket migrate into the dielectric, it can radically change the dielectric constant of the material. This means that capacitance and impedance will also change. And that will cause a dramatic rise in SRL. Bad news!

Testing:

One key difference between manufacturers is how or how often they test their cables. If it is precision video cable, for instance, every roll should be sweep tested. Ask what frequencies it is swept to. If it is swept below 200 MHz, it is unlikely that this cable was intended for digital video, which normally requires sweeping to 400 MHz or more.

Solutions:

Consider each company's market history. Ask other users. What is the company history? Many companies who have made wire and cable for many years, have only recently been making audio and video cables. What is there historic position in the audio and video industry? Do they offer a product warranty. What does it cover? How long is it? How long have they had a warranty?

FAILURE MODE TABLE

 

 

Analog Audio Digital Audio Analog Video Digital Video Broadband Machine Control Data
Installation Too hard a pull Too hard a pull Too hard a pull Too hard a pull Too hard a pull Too hard a pull
Exceed bend radius Exceed bend radius Exceed bend radius Exceed bend radius Exceed bend radius Exceed bend radius Exceed bend radius
Environmental Indoor version used outdoor Indoor version used outdoor Indoor version used outdoor Indoor version used outdoor Indoor version used outdoor Indoor version used outdoor
Operational wrong dielectric wrong dielectric wrong dielectric wrong dielectric wrong dielectric wrong dielectric
wrong connector
Manufacturing Excessive impedance variation Excessive impedance variation excessive SRL Excessive impedance variation

SUCCESS MODE TABLE
IDEAL CHOICES LISTED BELOW
DOES NOT APPLY TO PLENUM CABLES

Analog Audio Digital Audio Analog Video Digital Video Broadband Machine Control Data
Installation Pull within spec Pull within spec Pull within spec Pull within spec Pull within spec Pull within spec
Bend radius observed Bend radius observed Bend radius observed Bend radius observed Bend radius observed Bend radius observed
Environmental Correct indoor/outdoor construction Correct indoor/outdoor construction Correct indoor/outdoor construction Correct indoor/outdoor construction Correct indoor/outdoor construction Correct indoor/outdoor construction Correct indoor/outdoor construction
Operational polyethylene
polypropylene
foamed polyethylene solid
polyethylene
foamed polyethylene foamed polyethylene polyethylene
polypropylene
solid polyethylene
foamed polyethylene
Manufacturing foil coverage every roll swept every roll swept SRL specs every roll swept and tested

 

Choose the Best

Analog Audio Digital Audio Analog Video Digital
Video
Broadband Machine Control Data
Conductor copper
tinned copper
copper copper copper copper-clad steel copper
tinned copper
copper
Insulation/
Dielectric
PP
PE
PE PE
foamed PE
foamed PE foamed PE PVC
PP
PE
foamed PE
PE
foamed PE
Shield braid
foil
braid
foil
foil/braid
braid foil/braid foil/braid foil
braid
foil/braid
none
foil
Shield Material copper
tinned copper
copper
tinned copper
copper
tinned copper
foil+copper or tinned copper foil + aluminum
or tinned copper
foil
braid
foil + braid
none
foil
Jacket PVC PVC PVC PVC PVC PVC PVC
Features low capacitance 110ohms10.gif (838 bytes) impedance 75ohms10.gif (838 bytes) impedance 75ohms10.gif (838 bytes) impedance 75ohms10.gif (838 bytes) impedance varies 100ohms10.gif (838 bytes) impedance
U.S.
Standards
none AES/EBU SMPTE SMPTE SCTE Many TIA/EIA
European Standards none AES/EBU CCIR CCIR ? ? ISO/IEC