A Belden cable with no print is most likely a special order. You may find a small marker thread under the jacket (or braid). Counting the number of colored strands identifies the manufacturer. However, if the cable was designed for use with automatic stripping equipment, there may be no marker thread. then you will need to find the box, reel, or label from the cable.