Product FAQs
Quad Microphone Cable


Quad Microphone Cable Defined
Quad microphone cable, also called star quad, contains four wires instead of the normal twisted pair. The four wires are spiraled together and are color coded so that they can be combined for connectorization. The construction greatly improves common mode noise rejection.

Manufacturing of Quad Microphone Cable
Belden makes 1192A, available in 6 colors and we make a miniature version, 1804A, in 5 colors.

Wiring Quad Microphone Cable
To wire up a quad microphone cable, the four wires spiraled together are separated and stripped. Like colors are combined. That is, the two blue wires are twisted together and the two white wires are twisted together. The two resultant blue and white wires are then connected as a normal twisted pair.

How Quad Microphone Cables Works
Combining pairs in a spiral configuration affects what is called the "loop area". That means, the closer the wires stay together, the more likely that the noise and interference they encounter will be the same on each wire and the more likely the noise can be canceled by being a balanced line. Quad cable has the added advantage of having pairs of wires. They provide noise cancellation ("common mode rejection") at each pin, as well, due to the connection as a balanced line.