Product FAQ
Data Cable


The distance that Data cable can be run depends on a number of factors including the data rate, the capacitance of the cable, the structural return loss of the cable among other parameters. It is also dependent on the receiving device to error-correct, re-time signals or withstand attenuation of the data.