3-wire RTD
Belden does not make the RTD (Resistance Temperature Detector) itself, but many of our cables should be compatible with 4 wire RTDs. In general we would recommend a 3 conductor cable with an overall shield or cables made of multiple shielded triads. The device manufacturer can provide guidance as to what wire gauge to use and what distances are allowable.4-wire RTD
Belden does not make the RTD (Resistance Temperature Detector) itself, but many of our cables should be compatible with 4 wire RTDs. In general we would recommend a 4 conductor cable with an overall shield. The device manufacturer can provide guidance as to what wire gauge to use and what distances are allowable.