In a single mode fiber, the core is so small only one path length of travel for the photons is available for optical transmission. This is like the multimode example except our tube (fiber) is the same diameter as the BB (photon) allowing only one possible mode of travel.