New Generation Waterblocked series cables are intended for either indoor or outdoor applications. The multi-conductor cables use a waterblocking tape rather than a gel flooding compound, which allows for easier and cleaner terminations. The coaxial cables use Coreguard corrosion resistant compound. All cables use UV resistant jackets to further protect them from outdoor environments. (Note: These cables are not rated for direct burial. If they are installed underground, they must be placed in conduit. This is because these cables carry a CM rating necessary for indoor use.)
The multi-conductor cables can be used for a variety of applications such as security and alarm, audio and sound, intercom systems etc. The coaxial cables can be used for CATV, CCTV, MATV, etc.
Where are Waterblocked codes used?
Waterblocked New Gen codes are used where sound and security system wiring goes outdoors. This might be in underground troughs or other raceway, open air cantilevered shelters or other campuses where multiple buildings are interrelated. Educational buildings, administrative facilities, government buildings and other institutions are often arranged this way especially in the south, the gulf coast, and the southwest. For example, schools in the southern US frequently have open-air "hallways", classrooms with outdoor access, and large open spaces between interrelated buildings. Outdoor security systems, addressable fire alarm systems, intercom lines, cards access or other access control, and outdoor speaker lines are just a few examples.Can these cables be used for direct burial applications?
No, if these cables are buried, they must be placed in conduit.Who will use Waterblocked cables?
Anyone that is a current user of regular indoor New Generation cables probably has needs for outdoor cables as well, particularly if they are in a rainy, costal, or low lying area.