Splicing Optical Fibers

Preparation of Fibers

Preparation of fibers for splicing is very similar to the process described under connectorization. After jacket materials, strength members and buffer tubes have been cut to the appropriate lengths, the fiber buffer coatings must be removed.

Cleaving

After the buffer coatings have been removed, fibers must be cleaved in preparation for splicing. Cleaving is a method of breaking a fiber in such a way as to create a smooth, square end on the fiber.

Principles of Cleaving

Glass is typically strong until a flaw occurs and creates a region of high stress under pressure. The first step in the cleaving process is to create a slight flaw or "scribe" in the outer surface of the fiber.

Optical fibers can be scribed with a sharp blade of hard material such as a diamond, ruby, sapphire or tungsten carbide. The scribe is made by lightly touching the cleaned fiber, at a right angle, on the desired cleave point with a scribing tool. Only the lightest pressure is required to produce a scribe if the blade is sharp. NOTE: DO NOT USE A SAWING MOTION. A crude or slanted scribe will produce shattered or scalloped end surfaces.

After the scribe is made, a straight pull will produce the cleanest break. If bending accompanies pulling, a square break is less likely, especially with large fibers. Dispose of broken fiber pieces by placing them on a piece of tape. ALWAYS WEAR SAFETY GLASSES WHEN WORKING WITH OPTICAL FIBERS.

The level of quality required for a given cleave depends on the application. For fusion splicing, mechanical splicing and some connectors systems, cleaves must be nearly perfect. Some connector and splicing systems use cleaving to produce the final end surface on the fiber (no subsequent grinding or polishing). However, for quick continuity checks with a flashlight, less than perfect cleaves may be acceptable.

A 30x to 50x hand microscope is useful for quick checks of cleave quality.

Cleaving tools are available in inexpensive hand models or more sophisticated mechanized tools.

Splicing Methods

There are two basic types of splices: Fusion and Mechanical.

Fusion Splicing

Fusion splices are made by positioning cleaned, cleaved fiber ends between two electrodes and applying an electric arc to fuse the ends together. A perfusion arc is applied to the fiber while the ends are still separated to vaporize volatile materials which could cause bubbles.

Final precise alignment is done by moving fiber ends together until there is slight pressure between end surfaces.

An ideal fusion cycle is short and uses a ramped or gradually increasing arc current. A short, ramped cycle is considered least likely to produce excessive thermal stress in fibers. Cold temperatures require increased time and arc current.

Experienced operators consistently produce fusion splices with losses less than 0.2 dB per splice and averaging 0.3 dB on multimode fibers. Sophisticated fusion splicing systems for single-mode fibers produce typical splice losses of 0.05 to 0.1 dB.

Mechanical Splicing

Mechanical splicing systems position fiber ends closely in retaining and aligning assemblies. Focusing and collimating lenses may be used to control and concentrate light that would otherwise escape. Index matching gels, fluids and adhesives are used to form a continuous optical path between fibers and reduce reflection losses.

In-Line Connector/Connector Splicing

Connector-to-connector splicing may be used in situations where there is an abundance of optical power. Connectorized cable assemblies are joined through an alignment bushing which fits snugly over the tip of each connector.

Insertion losses for connector-to-connector splices can be as high as 1.0 to 1.5 dB. If these losses are considered excessive, an alternative method should be used.