Lease Table

The lease table shows you the IP addresses that the DHCP server has currently allocated.
The device displays the related details for every IP address allocated.

Tab. DHCP lease table

Parameters

Meaning

Possible values

Port

Module and port numbers to which this entry applies.

-

IP Address

IP address that the DHCP server has allocated to the device with the specified MAC address.

An IPv4 address from the pool.

Status

Status of the DHCP address allocation according to the Dynamic Host Configuration Protocol.

bootp, offering, requesting, bound, renewing, rebinding, declined, released

Remaining Lifetime

Time remaining in seconds until the validity of the IP address elapses, unless the client applies for an extension.

-

Leased MAC Address

MAC address of the client that is currently leasing the IP address.

Format xx:xx:xx:xx:xx

DHCP Relay

IP address of the DHCP relay via which the client has made the request.

IPv4 address or empty

Client ID

The client ID that the client submitted for the DHCP request.

a

Remote ID

The remote ID that the client submitted for the DHCP request.

a

Circuit ID

The circuit ID that the client submitted for the DHCP request.

a


Buttons

Tab. Buttons (Forts.)

Button

Meaning

“Reload”

Updates the fields with the values that are saved in the volatile memory (RAM) of the device.

“Help”

Opens the online help.