Containing more commercial AV than nearly any other professional venue in the world, Little Caesars Arena in Detroit, MI, holds 20,000 fans and utilizes state-of-the-art technology in every corner.

To bring all of this AV technology to life, there were three things Little Caesars Arena needed from an infrastructure standpoint:

1. Large Amounts of Fiber Cable

A fiber backbone (two 100G fiber connections) for the venue provides interconnections between access provider space, entrance facilities, equipment rooms, telecommunication rooms, telecommunication enclosures and buildings.

2. High-Performance Category 6A Cable

Belden 10GXS Small-Diameter Category 6A Cable provides a simple, compact design to make the most of available space without compromising performance. It supports 10G transmission speeds and saves up to 25% on space and weight.

3. Preassembled Data Center Cabinetry

For convenience – and to keep the project on track – all enterprise data center cabinetry and cable management systems arrived fully tested and assembled according to requirements.

Learn more by reading the blog in its entirety here!