Editor’s Note: This article was created with expertise from Tim Senkbeil, product manager at Lumberg Automation.

Thirty years ago most industrial control systems (ICS) were hardwired. Often sensors and actuators came with long wires already attached or individual wires that weren’t even jacketed together. Those wires would be threaded through conduits and then wired into the system. This was a time-consuming process that required the services of an electrician, costing organizations significant time and money.

The Hannover Fair of 1985 changed all that. M12 connectors were introduced and they stole the spotlight. Incorporating the use of the smaller M12 metric thread, they were initially released in 3-and 4-pin versions, with an IP67 rating. The M8 hit the market four years later, and soon both formats were standardized under IEC 61076-2-101, making them the standard for ICS.

A system that is linked up with M12 and M8 connectors makes assembling, testing and servicing ICS faster and less expensive. These advantages are further enhanced when a cord set is used instead of installing separate cables and connectors. Let’s take a close look at the advantages of M8 and M12 cord sets and the steps needed to select the right one.

M8 cord sets facilitate fast machine start-up time and easy maintenance

M8 cord sets facilitate fast machine start-up time and easy maintenance.

Save Time and Money During Installation and Maintenance

While the upfront investment of cord sets and connectors is greater than cables and wires, the cost savings comes from a reduction in labor and maintenance costs. A large system that might take a week to hardwire could be wired with connectors in as little as two days.

The savings resulting from reduced installation time is significant. Eliminating the need for an electrician further justifies the higher price point for M8 and M12 connectors.

New call-to-action

There is another advantage that you may not have thought of. Machine testing and start-up is faster. A lot of time spent during start-up is the result of miswired devices. Prewired and tested cord sets eliminate the majority of wiring errors.

Additional cost reductions come from reduced downtime, as cord sets can easily be replaced, again without need of an electrician. Connectorized sensors and actuators can also be replaced without rewiring the system.

1. Choosing the Right Cord Set – Start with the Environmental Needs

The possible combinations of cables and connectors is a surprisingly high number. Where do you even start the specification process?

Like most engineering decisions, there’s a balance between cost and performance. You want to choose the lowest cost option that meets the requirements of the application. For example, you don’t need armored cable if it is going to be run in wire trays in a temperature- and humidity-controlled environment.

Thus the first question to ask yourself is “How harsh is the environment for my project?” The answer to this leads to selecting the right industrial cable jacket and the right IP rating for the cord set. Below is a handy table that breaks down the options according to the harshness of the operational setting.

M8 Connector

Table 1: Select a cord set based on harshness of the application’s environment.

2. Determine the Connector Configurations

Since the introduction of the 3- and 4-pin versions of the M12 connector, many more variations and options have become available. While 4-pin M12 connectors are the most common, be sure to analyze your application and choose from:

  • straight or right angle configurations
  • 3-, 4-, 5-, 8- and 12-pin versions

For M8 connectors your options are:

  • Straight or right angle configurations
  • Snap(IP65) or screw connection (IP67)
  • 3-, 4- and 8-pin versions

3. Select the Keying Options

The M12 connector is also available in a variety of keying/coding options to further minimize wiring errors as follows:

  • A-code – Primarily used with sensors and actuators
  • B-code – PROFIBUS fieldbus connections
  • C-code (dual keyway) – Primarily used with AC sensors and actuators
  • D-code – 100Mb EtherNet/IP 4-pin
  • X-code – Gigabit Ethernet 8-pin

The following M8 connector configurations feature a keying/coding*:

  • B-code – PROFIBUS fieldbus connections
  • 8-pin version

Improve Reliability with the Right M8 or M12 Cord Set

The right cord set reduces installation time, wiring errors and machine start-uptime.

To select the best value cord set, carefully identify the harshness of the environment. Then select the appropriate cable shielding and cord set that will do the job.  There is no point in paying for a wash-down cord set for a material handling application.

Next specify the connector configuration(s) and, in the case of the M12 connector, the keying option(s).

Once production begins, if a sensor or actuator needs to be replaced it can be done quickly, minimizing expensive downtime. Your operation will benefit from maximum dependability and performance.

What is your approach to selecting M8 and M12 cord sets? I look forward to hearing your ideas.

*The M8 keying option information was updated on April 24, 2015.

New call-to-action

Related Links

Blog:  Wash-Down Cord Sets Improve Reliability for Sensor-Laden Automation Systems
Blog:  Marine-Certified Cables Improve Safety and Reduce Time to First Oil
Catalog:  PROFINET, EtherNet/IP and Ethernet Connectivity Solutions
Product Bulletin:  Lumberg Automation EtherNet/IP Modules for Industrial Automation Applications
Webpage: Connectors - Micro M12
Webpage:  Connectors - Pico M8