New stadiums and renovation projects are including AV, IT and security upgrades that can not only improve fan engagement, but also impact finances and reputation.

Today, AV is being used to provide things like:

  • Amenities and services that address the needs of fans
  • Technology that supports once-in-a-lifetime, interactive experiences
  • The ability to support fan engagement after an event

Modern stadiums are also finding ways to use AV to bring in additional revenue. Features such as augmented reality, letting fans select between different camera angles and the ability to view player stats instantaneously take game day to a whole new level.

Want to learn more about using AV as one way to monetize stadiums? Read the blog in its entirety here!