<img height="1" width="1" style="display:none;" alt="" src="https://px.ads.linkedin.com/collect/?pid=1363881&amp;fmt=gif">

Configurator-web

Broadcast Cable Assembly Configurators

Easily Build Your Assembly And Generate Quotes

Belden is continuing to build on its reputation as the solutions provider for the Broadcast and Pro AV markets, with the addition of pre-terminated, custom made, cable assemblies to its solutions portfolio.

Custom Broadcast Assemblies

Assembly configurators have been developed to help our customers navigate the breadth of cable and connector alternatives offered and to simplify the process of "building" assemblies that fit their particular installation requirements.

Once configured, each assembly will have a "SmartPart" number assigned to it that will allow the user to easily determine the construction of the assembly and can be used for repeat ordering. To facilitate the quoting process, the configurators have built-in functionality that allows the user to build a BOM of different assemblies that can then be sent in for quoting purposes.

Choose between four Assembly Configurators:

  • SMPTE Configurator
  • Audio Configurator
  • Tactical Fiber Configurator
  • Coax-Triax Configurator

Complete the form to download the configurators and start building your assemblies today.