St. Louis, Missouri – Dec. 12, 2018 – Belden Inc., a global leader in signal transmission solutions for mission-critical applications, is excited to announce new product solutions that are geared toward helping installers save time and money while end-users make the most of their enterprise network investments.

REVConnect FlexPlugs allow for quick connection of any IoT device using an RJ45 plug,
supporting connection in applications where the size of a typical field-terminated plug inhibits direct connection (MPTL) to IoT devices due to size and cable-routing constraints.

The 10GX REVConnect Wall-Mount System is a very high-density, Category 6A cross-connect system. Based on the REVConnect Coupler which allows for the use of cost-effective, cut-to-length cross-connects made of 10GXS Cable and REVConnect Cores, this system provides lower installation and maintenance costs as well as a very clean cross-connect field.

Fiber Raceways safeguard infrastructure investments with a tool-less, flexible system that snaps together quickly and easily for fast installation. An included design tool suite allows for quick configuration of networks, ensuring that no needed component gets overlooked.

XHW Wall-Mount Cabinets support IT/network hosting where space optimization is critical and floor mounting is not an option. Cabinets install quickly and easily to the wall, allow for left- or right-swing mounting. They also optimize equipment and cable management access and support up to 300 pounds of load capacity.

An expanded line of 4K UHD Coax Cables, including Mini RG-59, RG-11 and Flexible RG-6,
maximize 4K signal transmission distance on a single coax for 12G-SDI. They reduce weight and space requirements by 30% to 80%, depending on the application.

ReelTuff™ packaging protects Category cables and 4K UHD Media Cables with ruggedized, lightweight, “reel-in-a-box” packaging that provides superior resistance to crushing, puncturing, tearing and water. ReelTuff boxes allow multiple cables to be pulled vertically through stacked boxes and feature simple-to-read labels, descending length markings and easy-to-access, reinforced handles.

In addition, Belden is introducing Bulk Length Audio Cable to support large projects requiring custom length cable runs. Currently available are plenum, riser, waterblock and riser/waterblock cables. These audio cables can be used for permanent installation and are ultra-flexible for deployable applications.

To learn more about these solutions, and the types of technology and applications they support, visit www.belden.com/products/new-products.

Resolving signal transmission needs with IP- and legacy-based solutions that enable a smooth migration to convergence requires a universal approach for enterprise environments. Only Belden’s innovative enterprise connectivity solutions take this universal approach. Belden’s extensive portfolio spans LAN, data centers, building automation and security and access control to keep information running smoothly. Outstanding global service and support capabilities and application-specific warranty programs complete Belden’s unique offering.

About Belden
Belden Inc., a global leader in high-quality, end-to-end signal transmission solutions, delivers a comprehensive product portfolio designed to meet the mission-critical network infrastructure needs of industrial and enterprise markets. With innovative solutions targeted at reliable and secure transmission of rapidly growing amounts of data, audio and video needed for today’s applications, Belden is at the center of the global transformation to a connected world. Founded in 1902, the company is headquartered in St. Louis and has manufacturing capabilities in North and South America, Europe and Asia. For more information, visit us at www.belden.com or follow us on Twitter @BeldenInc.

For more information, contact:
Melissa Knapp
Media Relations
937.336.5258
Melissa.Knapp@Belden.com

Belden, Belden Sending All The Right Signals, and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden and other parties may also have trademark rights in other terms used herein.

Download Press Release