REVConnect Connectivity System line expands with Pre-Terminated Assemblies and Core Protective Caps

St. Louis, Missouri—Belden Inc., a global leader in signal transmission solutions for mission-critical applications, is excited to introduce two new REVConnect product line extensions to the ever-growing REVConnect Connectivity System.

As the first pre-terminated solution for applications that extend beyond the data center, new REVConnect Pre-Term Assemblies feature bundled cables terminated with the unique REVConnect universal core. This innovation allows for the smallest pre-term bundle footprint, making it easier to pull and install either in a data center or zone cabling application. The REVConnect Core provides installers with the flexibility to connect to either a jack or a plug – and lets end-users swap a plug for a jack down the road (or vice versa). When cable lengths can’t be defined, Core-to-Open pigtails can be used.

To improve installation flexibility and support a new time-saving installation method, the REVConnect Core Protective Cap allows installers to complete the REVConnect core termination and then use the cap to protect the terminated core until a jack or plug is installed at a later time. Installers and end-users no longer need to worry about contaminants impacting the performance of the pre-terminated run during ongoing construction or installation.

These two extensions represent continued innovation and support for the design flexibility needed to support IP-based devices and keep the Contractor in mind with easy-to-use timesaving installations.

Resolving signal transmission needs with IP- and legacy-based solutions that enable a smooth migration to convergence requires a universal approach for enterprise environments. Only Belden’s innovative enterprise connectivity solutions take this universal approach. Belden’s extensive portfolio spans LAN, data centers, building automation and security and access control to keep information running smoothly. Outstanding global service and support capabilities and application-specific warranty programs complete Belden’s unique offering.

About Belden
Belden Inc., a global leader in high-quality, end-to-end signal transmission solutions, delivers a comprehensive product portfolio designed to meet the mission-critical network infrastructure needs of industrial and enterprise markets. With innovative solutions targeted at reliable and secure transmission of rapidly growing amounts of data, audio and video needed for today’s applications, Belden is at the center of the global transformation to a connected world. Founded in 1902, the company is headquartered in St. Louis and has manufacturing capabilities in North and South America, Europe and Asia. For more information, visit us at www.belden.com or follow us on Twitter @BeldenInc.

For more information, contact:
Melissa Knapp
Media Relations
(937) 336-5258
Melissa.Knapp@Belden.com 

Belden, Belden Sending All The Right Signals, and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden and other parties may also have trademark rights in other terms used herein.