OZD Profi 12M G22 Enables Faster, More Reliable PROFIBUS Communications
St. Louis, Missouri - July 13, 2017 - Belden Inc., a global leader in signal transmission solutions for mission-critical applications, has released a new version of its PROFIBUS fiber optic repeater. The OZD Profi 12M G22 allows PROFIBUS networks to communicate over longer distances through fast and reliable fiber optic signals, while also guaranteeing signal reliability through integrated redundancy technology.
“Control networks need real-time communications that are extremely fast and highly reliable. This combination can be achieved through devices, such as our OZD Profi 12M G22, that place a priority on data integrity and high speeds,” said Rolf-Dieter Sommer, product manager at Belden. “With data transfer rates up to 12 Mbps, our new repeater is among the fastest in the world. And, if a fault were to occur, its built-in ring redundancy will automatically switch over to another ring segment for maximum reliability.”
This new device builds on the proven family of Hirschmann PROFIBUS repeaters with higher signal conversion capacity. Specific enhanced capabilities of this repeater include:
This PROFIBUS fiber optic repeater is ideal for real-time control networks that extend across long distances. It is useful in energy applications, such as oil and gas production or pipelines, and in the transportation industry, such as in highway traffic control systems. Other uses include water and wastewater systems and manufacturing systems that require large PROFIBUS communication networks that are reliable and safe.
For more information on the OZD Profi 12M G22 Fiber Optic Repeater, visit www.hirschmann.com/en/Hirschmann_Produkte/Industrial_Ethernet/news/OZD_Profi_12M_G22/index.phtml.