Single Pair Ethernet (SPE) - Less is More
Single Pair Ethernet in combination with Time-Sensitive Networking and Power over Data Lines enables an end-to-end Ethernet network from the sensor to the cloud and will be used anywhere where space is limited and the weight of cables and components plays a major role.
Topics Covered in the Webinar:
- What are the drivers urging for SPE - a quick history lesson
- Why SPE is the missing link in field network connectivity
- Use case examples of Single Pair Ethernet
- The 6 key points to stay ahead of the game