Enable Data Center Flexibility, Manageability, Scalability and Security
Advances in Multi-Fiber Connectivity
What Is This White Paper About?
Part 1: Reducing Optical Loss in Multi-Fiber Connectivity
Today’s data centers are looking to deploy infrastructures that are ready to support 40- and 100-gigabit Ethernet (GbE) as well as flattened data center architectures to improve low-latency, server-to-server communication. Supporting these higher speeds and new designs is causing optical insertion loss budgets to shrink. To date, the loss values for many preterminated multi-fiber (MPO) solutions have only allowed for two mated pairs in an optical fiber channel. This has significantly limited the ability for data center managers to deploy flexible, manageable, scalable and secure networks.
Part 2: Optimizing Data Center Design with Low Loss Multi-Fiber Connectivity
Insertion loss is a critical parameter that determines the maximum distance of an optical fiber channel for a given transmission rate. With reduced maximum channel loss for 40 and 100 GbE, the loss values on multi-fiber connectivity have become more critical than ever, especially when deploying multi-point architectures. Remember, both 40 and 100 GbE now have a total connector loss limit of 1.5 dB and 1.0 dB respectively. Connector loss is directly related to how many mated pairs can be placed within a channel. However, deploying 3-, 4- or even 5-point architectures allow data center managers to get back to the basic, fundamental and time-honored best practice of convenient cross-connects and zone distribution areas (ZDAs) that provide significant benefits in flexibility, manageability, scalability and security.
Topics covered in the White Paper:
Part 1
- Reducing Optical Loss in Multi-Fiber Connectivity
- Media and Connectivity Choice Matters
- Why MPO-24 Falls Short on Loss
- Belden is Leading the Way
- New Standards Have an Impact
- Why Does Insertion Loss Matter?
Part 2
- Optimizing Data Center Design with Low Loss Multi-Fiber Connectivity
- 2-Point Simple Channel Architecture
- 3-Point Architecture
- 4-Point Architecture
- 5-Point Architecture
- Belden Gets You There
Download the white paper to learn methods you can start deploying immediately to optimize your data center.