When something breaks or isn’t working right, the instinct for most hotel operators is to move quickly to take care of the problem. In most cases, that means scrambling to find a single product that will resolve the issue (at least temporarily).
Guests complaining about poor Wi‑Fi connectivity? Add more access points. Cameras at the edge don’t have power? Drop in a small switch or PoE injector. Meeting rooms with legacy copper or coax? Pull new cable.
But taking a shortcut now—or not verifying existing hotel network infrastructure before adding something new—means paying for it later.
While every purchase is meant to address a specific challenge, it also adds another vendor, another trade and another schedule to coordinate. This makes the network more complicated to build, maintain and scale. And no one is thinking about or accountable for the big picture or long-term vision.
The hidden cost of solving problems one device at a time
To guests, these individual upgrades may make the property feel modern. Behind the scenes, however, your team is responding to complaints, working around operational bottlenecks and managing tech projects that never catch up. And it’s all because problems are being treated as isolated issues instead of signs that the hotel network infrastructure needs attention.
This pattern turns into technical debt. And it accumulates when quick fixes are the default. If you’re taking care of today’s problem with a local workaround, then every future change will be harder and more expensive because you have to deal with all the shortcuts and patches that came before.
Future costs could come in the form of:
- Increased maintenance and risk
- Longer, more disruptive upgrades
- Greater reliance on the few people who understand how these piecemeal products work
- More integration and troubleshooting whenever something new is added
- Lost revenue when rooms or spaces can’t support new services fast enough
How network design holds back guest-facing design
Technical debt also ties up value in systems and platforms you’ve paid for but can’t fully use, which means they aren’t delivering the return you expected.
Think about guest‑facing systems: in‑room entertainment, mobile check‑in, room controls, etc. Each system is meant to improve guest satisfaction or protect average daily rate (ADR) and bookings. But if the underlying hotel network infrastructure wasn’t designed with those workloads in mind as you rolled them out, they become unreliable because they put too much strain on the network or team.
Or perhaps a room platform or mobile check‑in app is deployed, but key features stay turned off and the system never delivers what you paid for. Why? Because enabling those features would require touching cabling, closets and edge components that were added in a piecemeal approach, potentially turning a simple change into a risky construction project.
The downtime risk hiding in one‑off projects
Beyond accumulating technical debt, one-off projects also impact downtime.
Most hotel upgrades are happening while you’re trying to keep rooms open, protect ADR and bookings during long refresh cycles, and avoid shutting down revenue‑generating spaces.
Isolated fixes don’t keep your property running smoothly over the long-term. Instead of helping you avoid downtime, they become possible points of delay when you want to change something or roll out a new system.
Every small workaround creates another touchpoint that has to be understood and managed the next time that area or system is updated. When that project comes along, work stops and starts as different trades and teams try to sort out what’s there, decide what they can reuse and look for ways to make the new systems work with what’s already in place.
Choose solutions that simplify your network, not add to it
For hotels that are ready to start paying down their technical debt, the first step is this: Stop trying to solve every problem at the device level and start thinking about how work and guest experiences actually happen.
This doesn’t mean never buying another component. It means evaluating options based on how they affect your network and current operations. Solutions that can reduce the number of separate components, pathways, contractors, vendors and handoffs move you toward a network with less technical debt and less downtime.
When the next refresh or expansion comes along, you’ll be working with hotel network infrastructure that was meant to be changed, updated and scaled … not unraveling years of one-off fixes to make room for the next change.
Let business goals drive hotel network decisions
How do you break the cycle?
There is no universal way to fix technical debt because no two properties carry it the same way. For example, the decisions made during a 2015 refresh, the vendor you locked in during a 2019 renovation and the workarounds added during the pandemic are yours specifically.
Start by working with the infrastructure you already have and thinking about the KPIs and outcomes you need to improve. Guest satisfaction, average room rate and bookings, and operational efficiency are universal measures that should be used to guide every network and infrastructure decision.
Define the business goals for your project and work backward. Those will look different for every property. If your objective is to improve guest‑satisfaction scores and ADR, then what kind of in‑room experience and connectivity do you need to deliver? And how will you get there with as little disruption and rework as possible?
Asking questions like these naturally results in a closer look at existing hotel network infrastructure to see:
- What can safely be reused?
- What can be standardized?
- What needs to be upgraded?
- How can work be sequenced?
This perspective also makes it easy to understand how much technical debt you’re carrying.
For instance, if you can’t turn on features in an existing in‑room system without triggering the need for cabling upgrades, closet work and changes at the edge, then you’ve learned something about your current design: It wasn’t built with those workloads in mind.
Belden is your partner in reducing technical debt
Each project is an opportunity to reduce technical debt if it’s handled as part of a broader plan and strategy. Over time, you’ll end up with hotel network infrastructure that supports how you operate without having to deal with decisions made years ago that limit what you can do. You’ll be able to deliver the experiences and revenue your network was supposed to support in the first place.
Belden helps you design and integrate modular, scalable solutions instead of one‑off products. As your one-stop shop for complete connection solutions, we’ll find ways to address your unique requirements and unlock new possibilities while simplifying purchasing, coordination and accountability.
It starts with an assessment of your existing network and physical infrastructure. What cabling runs do you have that could be repurposed? Where are your IDFs, and do they need to be there? Is your cabling system being asked to do more than it was designed for? Do you need to add new runs to scale your network? Those answers will help everything that comes next … including whether you need new infrastructure at all.
Ready to deploy solutions that reduce complexity, downtime and technical debt across your property?