Certification-Training-Hero-Belden-2020-09

Certification ISO 14001

 ISO 14001 Icon for Green Inititiatives page

ISO 14001 is an internationally recognized standard for environmental management.

The standard describes the controls required for those business activities which impact the environment; including use of natural resources, waste management, and energy consumption.

Through the development of an environmental management system, which meets the requirements of the standard, an organization is able to:

- identify and control the environmental impact of its activities, products or services
- continuously improve its environmental performance
- implement a systematic approach to setting and achieving environmental objectives and targets

Certificates:
ISO 14001 - Belden Deutschland GmbH and Hirschmann Automation and Control GmbH
ISO 14001 - Belden Deutschland GmbH and Hirschmann Automation and Control GmbH (German)
ISO 14001 - Belden Wire & Cable B.V.

 

ISO 27001

ISO/IEC 27001:2022 Hirschmann Automation & Control GmbH

 

OHSAS 18001

OHSAS 18001 Icon for Green Inititiatives pageBS OHSAS 18001 is an internationally recognized standard for occupational health and safety management.

The standard describes the controls required for those business activities which impact health and safety of employees.

Through the development of an occupational health and safety management system, which meets the requirements of the standard, an organization is able to:

- identify and control the health and safety impact of its activities.
- continuously improve its health and safety performance
- implement a systematic approach to setting and achieving health and safety objectives and targets

For more information:
www.bsigroup.com


ISO 50001

ISO 50001 Icon for Green Inititiatives pageISO 50001 is the international standard for Energy Management Systems, created by the International Organization for Standardization (ISO).

The standard specifies the requirements for establishing, implementing, maintaining and improving an energy management system, whose purpose is to enable an organization to follow a systematic approach in achieving continual improvement of energy performance, including energy efficiency, energy security, energy use and consumption.

Certifications:
ISO 50001 - Belden Deutschland GmbH and Hirschmann Automation and Control GmbH

 

 

REACH

Reach Icon for Green Inititiatives pageREACH is the Regulation for Registration, Evaluation, Authorization and Restriction of Chemicals.

It entered into force on 1st June 2007 with the intention of streamlining and improving the legislative framework on chemicals within the European Union (EU).

REACH places greater responsibility on industry to manage the risks that chemicals may pose to the health and the environment.

The stated aims of the legislation are to:

- improve the protection of human health and the environment from the risks that can be posed by chemicals
- enhance the competitiveness of the EU chemicals industry, a key sector for the economy of the EU
- promote alternative methods for the assessment of hazards of substances
- ensure the free circulation of substances on the internal market of the European Union

More Information can be found on
ec.europa.eu
echa.europa.eu


REACh Confirmations:
Belden Deutschland GmbH
Hirschmann Automation and Control GmbH
Belden Deutschland GmbH (German)
Hirschmann Automation and Control GmbH (German)

 

SCIP Reporting Responsibility

SCIP Icon for Green Inititiatives page

 

Belden is conscious of its responsibility under the updated Waste Framework Directive (EU) 2018/851 and is continuously working on the implementation of the SCIP notification obligation. Until we have completed the compliance processes and acquired all data from our upstream suppliers, we kindly ask you direct your questions to Sales Support.


 

 

 

 

Declaration for California Proposition 65

CP65 Icon for Green Inititiatives page


Proposition 65 (formally titled The Safe Drinking Water and Toxic Enforcement Act of 1986) is a California law passed by direct voter initiative in 1986 by a 63%–37% vote. Its goals are to protect drinking water sources from toxic substances that cause cancer and birth defects and to reduce or eliminate exposures to those chemicals generally, such as consumer products, by requiring warnings in advance of those exposures.

 

 

 


Declaration for California Proposition 65
:
Belden Deutschland GmbH
Hirschmann Automation and Control GmbH

 

WEEE

WEEE Icon for Green Inititiatives pageThe Waste Electrical and Electronic Equipment Directive (2002/96/EC) became European Law in February 2003. The directive sets targets for the collection, recycling and recovery of all types of electrical goods.

The directive imposes responsibilities for the disposal of waste electrical and electronic equipment on the manufacturers of such equipment.



For more information
:
ec.europa.eu

 

RoHS II


RoHS Icon for Green Inititiatives pageThe Directive on the Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment was adopted by the European Union in February 2003 and took effect on 1 July 2006.

This directive bans the placing on the EU market of new electrical and electronic equipment containing more than agreed levels of lead, cadmium, mercury, hexavalent chromium, polybrominated biphenyl (PBB) and polybrominated diphenyl ether (PBDE), Bis(2-ethylhexyl) phthalate (DEHP), Butyl benzyl phthalate (BBP), Dibutyl phthalate (DBP), Diisobutyl phthalate (DIBP) flame retardants.

RoHS Declaration for Directive 2011/65/EU and supplement 2015/863/EU:
RoHS - Belden Deutschland GmbH
RoHS - Hirschmann Automation and Control GmbH
RoHS - Belden Deutschland GmbH (German)
RoHS - Hirschmann Automation and Control GmbH (German)

China ROHS


China Icon for Green Inititiatives pageThe Administrative Measure on the Control of Pollution Caused by Electronic Information Products is a Chinese government regulation to control certain materials, including lead.

Legislation applies to electronic information products and includes products imported into China for sale.
It provides a framework for substance restrictions, certifications, labeling, and information disclosure.

The confirmations are enclosed with the product. For Belden Deutschland GmbH (Lumberg Automation and Hirschmann Connector products) please request via the Help Desk.