Related Tags
- ANSI/TIA-568.5: Single-Pair Ethernet. The standard is expected to provide specifications for cables, connectors, cords, links and channels using one-pair connectivity.
- Telecommunications Systems Bulletin: Optical Fiber Channel Polarity. TIA is working on a Telecommunications Systems Bulletin that will make fiber polarity far easier to understand.
- ANSI/TIA-942-B.1: Edge Data Centers. Data centers can now be transportable, portable or built outside of a traditional building envelope. The ANSI/TIA-942-B.1 standard will provide guidance on design and development for these new types of edge data centers.
Want to learn more? Read the blog in its entirety here!
About the author
Henry Franc
Field Applications Engineer
With an emphasis on data center design, planning and building, Henry Franc acts as a trusted advisor for large or complex projects across all verticals assessing clients’ business needs and finding the best technology options to meet them. He was also elected by industry colleagues to serve as vice-chair of the TR42 Telecommunications Cabling Systems Engineering Committee.