Futuristic Concept: Big Data Center Chief Technology Officer Holding Laptop, Standing In Warehouse, Information Digitalization Lines Streaming Through Servers. SAAS, Cloud Computing, Web Service

As AI matures and scales, organizations have to decide: Where will these high-density workloads run?

For many, AI started in the cloud, but it isn’t always staying there. Data center and infrastructure teams are realizing the latency, cost and control tradeoffs that result when all AI processing is pushed to hyperscale facilities.

Accordingly, more AI workloads are moving back into enterprise and colocation environments. But there’s one problem with this shift: These environments were built long before AI was in use, and their power and cooling profiles can’t handle this level of density.

Not all organizations have the capital (or the desire) to construct new data center spaces every time AI demand spikes. And, especially within enterprises, their teams don’t have the expertise or time to design new high-density solutions for each new project.

Factors to consider when deciding where AI will live

When enterprises started to deploy AI, it initially made sense to lean heavily on cloud and hyperscale providers. Capacity was available, resources could be scaled quickly and experimenting with pilot projects was fast and low-risk.

With AI moving from small, contained proofs of concept to large-scale, always-on services, running workloads offsite isn’t always the best way to support fast, reliable access. That’s why more teams are looking for ways to meet AI requirements within the data centers they already operate.

As data center and IT leaders decide which AI workloads should run where, three factors need to be considered: how quickly AI services need to respond, what kind of data they interact with and how predictable their long‑term cost and capacity needs must be.

 

1. How quickly does AI need to respond?

Many AI applications are latency‑sensitive, which means they depend on fast, consistent response times to be effective. This includes applications like:

  • Fraud detection in financial transactions
  • Smart building controls that adjust heating, cooling and lighting based on occupancy and environmental conditions
  • Real‑time personalization in customer‑facing digital experiences
  • Smart campus operations that coordinate energy use, space utilization and services across buildings

In these instances, sending data to a remote data center and waiting for a response can add delays that operations can’t tolerate.  

Bringing a portion of the AI stack closer to where critical data is generated and consumed helps reduce latency so performance and user experience can be maintained. 

 

2. Where does it make the most financial sense for AI to run?

Cost is another factor bringing AI back to enterprise and colocation facilities. High‑density GPU clusters that run 24/7 can be expensive to host in the cloud.

Many organizations reach a point where it makes financial sense to keep certain work in hyperscale environments while relocating mission‑critical workloads into infrastructure they control. The reason: more predictable cost and capacity planning. Teams can better forecast spend across hardware lifecycles, avoid surprise consumption spikes and manage budgets and upgrades.

 

3. What types of data will AI need to use?

AI relies on training and inference to turn raw data into decisions that matter to the business. These activities involve large, sensitive datasets that enterprises don’t always want to move to external environments due to regulations, internal policies or even customer expectations.

Running AI in enterprise or colocation data centers helps organizations protect critical data by keeping it close, simplifying compliance and reducing the operational overhead associated with moving data back and forth. 

Adapting existing data center spaces for AI

Bringing AI in-house means asking spaces that have fixed power, cooling and space constraints to support a new set of requirements.

While some data centers may have room for more racks, these racks are now filled with GPUs, which draw several times more power per rack than the space was built for. Finding a way to deliver another 20 kW to 40 kW and beyond—and removing the associated heat at the rack—is a different story. Traditional cooling sized for legacy loads often struggles to keep high-density AI clusters within safe operating ranges without overcooling the rest of the room or creating hot spots.

The keys to keeping up with shifting demands

In addition to handling density, the teams bringing at least some AI in-house must also plan for flexibility. AI is moving fast, and its power and cooling requirements are changing quickly, too.

Data center operators need to be able to add more or change high-density compute as demand grows without rethinking the entire space every time.  

This means deploying solutions that can:

  • Support higher rack density
  • Coexist with legacy equipment
  • Work with multi-vendor server, storage and networking choices
  • Be deployed in specific aisles or pods without a full mechanical overhaul
  • Tie into existing power and cooling infrastructure where possible
  • Scale in modular, repeatable “blocks” as additional capacity is needed

Bringing cooling to the rack supports AI  

As densities climb, taking a rack-level approach to power and cooling is critical; AI clusters concentrate more power into fewer racks. Instead of asking the whole room to absorb the heat load, rack‑level cooling moves this handoff point to the rack.

Rear‑door heat exchangers attack the problem at the source. A cooled rear door captures and removes the heat as it leaves the rack instead of letting hot exhaust spill into the room.

For retrofit projects especially, this is a big deal. Rear‑door and other rack‑level solutions can often be added to existing rows with minimal disruption inside a live environment. You can increase density exactly where and when you need it to support critical workloads.

Belden and OptiCool enable AI-ready infrastructure

To address these challenges, Belden and OptiCool are partnering to create integrated rack‑level solutions that make it possible for enterprises and colocation operators to support high-density AI workloads inside their existing facilities—or inside new ones.

By integrating OptiCool’s rear-door heat exchangers with Belden’s racks and cabinets, advanced cooling can now be brought straight to the rack to deliver reliable, scalable, AI-ready data center operations. When paired with Belden’s high-speed, low-latency networking cabling and power distribution, the full rack performs reliably, even in mixed IT/OT environments.

OptiCool’s rear-door heat exchangers remove heat at the source. Its active RDHx uses two-phase refrigerant technology: variable-speed fans pull hot exhaust through evaporator coils in the door, capturing up to 120 kW of heat per rack before it enters the white space. A dedicated refrigerant loop carries the heat to an external rejection unit. As a result, far less heat burdens existing CRAC/CRAH units or chillers, reducing energy use and enabling safe, high-density operation alongside existing infrastructure.

See how OptiCool simplifies high-density data center cooling.

With this high-density, rack-level cooling option, teams don’t have to dedicate time or expertise to designing and integrating their own AI-ready infrastructure—or commit capital to building a new facility to accommodate demanding workloads. Because these solutions are delivered as a package (racks, power, connectivity and cooling), they can be deployed quickly, without the complexity associated with traditional design and integration.

Together, we can help you determine which AI workloads need to move closer to data and users—and the best ways to support them. Find us at Data Center World, 2026 Booth #437, to see a Belden rack fitted with an OptiCool 60 kW rear door heat exchanger, in addition to other data center solutions.

Learn how we can help

 

Related Links

AI-driven data centers build the backbone of our digital future

Why building a data foundation matters in AI for manufacturing

Data center resilience is about evaluating risks and adapting practices