As a result of these changes, Power over Ethernet (PoE) is also on the rise. In fact, BSRIA predicts that more than 80% of wireless access points (WAPs) will rely on PoE as a way to transmit electrical power and data to remote devices over standard twisted-pair wire in an Ethernet network by 2020. Between 20% and 50% of other devices and applications – security cameras, access control systems, lighting and HVAC – are predicted to rely on PoE by 2020.
Taking the “Direct-Connect” Approach
As LANs transform and grow to accommodate these changes, simplicity will be key to avoid cumbersome installation and scaling challenges, and save time.
Using security cameras as an example, LAN infrastructure can be simplified when plugs are placed on the end of horizontal cabling and run straight out to an IP device. PoE cable can be directly connected to a camera without any connections in between – in this situation, it doesn’t make sense to deploy several other connections along the way.
This simplified type of connection method is one we like to call “direct connect.” It’s also known as a home-run connection or an end-to-end connection. This direct-connect method efficiently connects IP devices to the LAN. A single cable is used to connect a device at one end; the other end of the cable is connected directly to where it needs to be.
When you utilize horizontal cabling in this fashion, two things happen:
- More efficient power delivery due to solid, larger-gauge cable construction that permits higher output without applying additional power from the source
- Minimal insertion loss because the heat risk from bundles downstream is reduced
Direct-Connect Testing
Main Tester- Remove Unite
- Permanent Link Adapter
- Coupler
- Link Under Test
Although a direct connection can improve efficiency, simplify infrastructure and reduce complexity, there’s an important point to keep in mind: You can’t measure the performance of a plug using channel specifications on your field tester.
Channel specifications don’t include the plug on the end of the channel. When using a field tester with channel adapters for channel testing, the plug is essentially “subtracted out”; as a result, you didn’t get to see the performance of the plug on the end of your cable. Because direct-connect cabling likely uses field-attach plugs, a slight modification to the field test is required, using pigtails, to ensure that the plug was installed correctly.
Alternatively, you can use ISO test limits, which are available on testers labeled as TR11801-99-2. This method utilizes patch cord adapters, and does the calculation to include the plug on the end of the channel.
Direct Connect and Grid Cabling
Using a direct-connect method in combination with grid cabling will bring you the same benefits as an entire direct-attach assembly. In this scenario, horizontal runs are pulled to zone boxes. Within these zone boxes are patch panels. Assemblies are deployed from these boxes/panels to connected devices: WAPs, lights, monitors, cameras, printers, displays, etc. When devices are added or moved, the assembly from the box to the static end device is the only thing that needs to be changed. (Check back in a few weeks to learn more about grid cabling in a new blog post.)
To better support direct-connect field assembly, Belden is releasing a new product this month that’s ideal for use with bonded-pair cabling. A core that accepts either a plug or a jack body is installed on the cable, providing an added level of versatility and reliability to support the ever-evolving LAN. The product is optimized for connectorizing horizontal cabling with either a plug or a jack.
Make sure you sign up for our blog to be the first to hear about this new Belden product.
About the author
Ron Tellas
Sr. Solution Architect, Enterprise Solutions, Belden
Ron Tellas is a subject-matter expert in RF design and Electromagnetic Propagation and joined Belden in 2016 to help define the roadmap of technology and applications in the Smart Building. He now takes these experiences to incorporate systems, equipment and connectivity into network solutions. Ron represents Belden in several standards organizations, committees of the National Electrical Code and as a board member of the FMP Alliance. He has a master and bachelor degrees in electrical engineering, a master in business administration and the inventor of 17 US patents. Ron is a proud recipient of the 2024 Harry J. Pfister award for his outstanding and impactful contributions to the Telecommunications Industry.