Data centers are quickly becoming some of the most demanding but least flexible loads on the power system. It’s a dynamic that every utility is wrestling with right now.
As part of the work Belden’s doing with utilities and large energy users, I was recently part of a Utilities Technology Council (UTC) data center discussion that brought together electric cooperatives, investor-owned utilities and telecom experts to talk about hyperscale growth and what it means for the grid.
While the conversation reinforced a lot of what those of us in the room already knew, it also introduced new angles and pressure points. Data center power design decisions are now a grid-level concern, and it all comes back to this: AI‑driven demand is arriving faster than generation, transmission and interconnection processes were designed to handle. Hyperscalers operate with a “move fast, iterate quickly” mindset, but utilities do the opposite: They focus on reliability and safety. As one participant put it, “Data center operators are playing 3D chess, while utilities are playing checkers.” The tools, processes and risk tolerances on each side are very different.
From my perspective, that sentiment captures the heart of the challenge. Data centers and AI are pushing the boundaries of what energy infrastructure can support, while utilities are working hard to respond. Bridging that divide will require more transparency, engagement and shared planning.
Here are a few other takeaways from the discussion that data center leaders and energy stakeholders need to understand. While we don’t have all the answers today, these themes give us a clear view of where collaboration and investment need to focus next.
How much power does a data center require? More than the grid was built to deliver
Just a few years ago, the answer to “How much power does a data center require?” was measurable in tens of megawatts. During the UTC data center discussion, however, several utilities described a pipeline of hyperscale projects that would’ve been hard to imagine even just a few years ago. One cooperative talked about more than 20GW of data center load expressing interest in its territory. This number is enough to reshape any resource plan. Individual requests for capacity now range from 100MW to multi‑gigawatt campuses, often with expectations for power in three to five years. Today’s workloads have pushed data center power density to levels that change what utilities are being asked to support.
That kind of demand forces utilities to revisit planning assumptions and system peaks. Where and how can these large blocks of new load be connected without compromising reliability elsewhere? It’s a question that doesn’t have a simple answer.
Planning horizons and developer timelines don’t match
Traditional utility planning looks out decades at a time. But hyperscalers and large data center developers operate within much shorter time horizons—and they want power to line up with their fast go‑to‑market schedules.
Panelists highlighted projects where the construction phase has taken up to four years … and that doesn’t include the time required to bring new generation online.
New gas plants can be eight to 10 years out due to permitting and pipeline constraints. Large transformers, breakers, turbines and pad‑mount units are on order for years, with little room to compress timelines. The message from the utilities in the room was clear: No amount of capital or urgency can shortcut the physical and regulatory work required to add that much capacity.
Both sides have to plan differently and engage in early conversations about data center power design. Utilities are starting to push for earlier signals about real projects vs. speculation, and they’re asking hyperscalers to involve them sooner in the planning cycle.
Reliability is under pressure as extreme weather intensifies
Extreme weather is already testing the limits of today’s grid, even before large data center loads are fully in the mix. Case in point: In early February, all four balancing authorities in the Carolinas hit all‑time winter peaks on the same day. Residential heating load spiked as a result, and system operators had to make hard decisions to keep the lights on.
As hyperscale demand grows, these large new loads could make it harder to maintain reliability if they aren’t integrated carefully. Legislators and regulators are already talking about mandatory curtailment for data centers and other large industrial customers during emergencies to make sure life‑critical load remains the priority. For utilities, that means building in the ability to curtail while still honoring contracts and maintaining long‑term relationships with large customers.
Hyperscalers are exploring their own power generation
Another theme is the growing interest in “bring your own power” for large data centers. Faced with long timelines for new grid‑connected generation, hyperscalers are now looking at options like onsite gas turbines, distributed generation, nuclear microreactors and large‑scale backup solutions. While this could be a potential relief valve for some parts of the grid, it also brings a new set of coordination challenges.
If more generation sits behind the fence, utilities will need clear visibility into how and when that capacity operates, how it interacts with the bulk system and what happens during abnormal conditions. There’s also a regulatory dimension to consider: Current rules don’t always accommodate these new models in some jurisdictions, so utilities, regulators and large customers will have to find ways to work together to keep the system stable.
Speculation and screening are now part of the job
Not every data center inquiry that hits a utility’s inbox is coming from a hyperscaler. Several participants describe a growing wave of speculative real estate activity. In other words, developers want to secure interconnection positions “just in case,” with no specific customer in mind.
To protect existing members and customers, many cooperatives are tightening interconnection processes, requiring higher levels of financial commitment upfront and creating new rate structures to isolate the impact of large new loads. The goal is to make sure they don’t have to subsidize projects that may never materialize.
How utilities can prepare for what’s next
The UTC data center discussion reinforced the fact that hyperscale demand is creating a long‑term shift in how and where energy is consumed.
For utilities, that means:
- Updating planning processes to account for very large, fast‑arriving loads
- Investing in grid modernization, automation and communications so operators have visibility
- Working with regulators to create frameworks to support new generation models and standby resources
- Strengthening coordination with data center operators so the grid and facilities stay aligned
- Engaging earlier on data center power design decisions go generation and interconnection plans align from the start
As these pressures continue to build, Belden is here to help you build infrastructure that can keep up with this wave of demand without sacrificing reliability. We find ways to deliver secure, dependable and affordable energy with complete connectivity solutions that help energy teams operate faster, safer and smarter.