Dark purple streak waves on purple background

St. Louis, Missouri – November 20, 2025 – Belden Inc. (NYSE: BDC), a leading global provider of complete connection solutions, today announced the launch of new products designed to enhance performance, security and reliability across automation and smart infrastructure environments.

Belden Industrial Access Point and premium cables
New product releases include the first Belden Industrial Access Point for deterministic, low-latency Wi-Fi 7 and a range of premium cables and products to meet evolving automation and smart infrastructure demands.

 

  • Belden RemoteIP Indoor/Outdoor CMR/CMX Cable is backed by Belden’s expertise in manufacturing premium products and meets IEEE 802.3 application standards. The RemoteIP Cable achieves 10 Mb/s transmission at 215 meters, 100 Mb/s transmission at 200 meters, and 1 Gb/s transmission at 130 meters.

  • Belden Fire-Resistant Safe-T-Line LPCB rated Cables with Stranded Conductors combine LPCB-certified safety with rapid installation. Built with stranded conductors for superior flexibility, these cables meet BS 6387 CWZ and EN 50200 standards for proven reliability under fire and offer unique toolless strippability to significantly reduce installation time.

  • The new Belden Industrial Access Point delivers deterministic, low-latency Wi-Fi 7 for robotics, logistics and automation. Get dual-concurrent 5 GHz/6 GHz, fast roaming and built-in diagnostics for seamless connections that help disparate systems work in harmony.

  • Belden DataTuff Mining Grade Fiber Cable is designed for longevity and low maintenance. The cables resist rodents, abrasion, impact, fungi and fire, while supporting real-time safety monitoring and seamless connections that unlock new possibilities across every layer of mining operations.

  • Lumberg Automation M12 Push Pull Cordsets now feature new angled variants. The M12 Push Pull Cordset installs easily, even in tight spaces, without tools or screwing in. It conforms with IEC 61076-2-010 and meets standards for vibration and external force resistance.

  • The Belden Single Pair Ethernet (SPE) REVConnect FlexPlug revolutionizes commercial building connectivity by simplifying single-pair Ethernet installations for smart building applications, enabling extended reach and space savings.

  • Hirschmann 19” rack mount GREYHOUND 125/126 Ethernet Switches create better connections and boundless possibilities, streamlining installation and lowering total cost of ownership via PoE—no extra power supplies needed.

  • The Belden IAF-240 Industrial Firewall now integrates with Industrial HiVision Network Management, features an optional Intrusion Prevention Pro module, and offers flexible software subscription extensions. This next-gen industrial firewall provides enhanced control, scalability, and long-term value.

  • Belden Waterdog New Generation Direct Burial Cables facilitate better connections between in-building and outdoor devices. Rugged Waterdog cables feature water-blocking material to withstand harsh conditions.

  • macmon NAC version 6.4.0 enhances network security and simplifies management with new Ethernet/IP capabilities for OT environments and EAP-FAST for stronger 802.1X authentication, ensuring only authorized devices connect and effectively limiting attack surfaces in converging IT/OT networks.

Learn more about these products, as well as the technologies and applications they support.

 

About Belden

Belden Inc. delivers complete connection solutions that unlock untold possibilities for our customers, their customers and the world. We advance ideas and technologies that enable a safer, smarter and more prosperous future. Throughout our 120+ year history we have evolved as a company, but our purpose remains – making connections. By connecting people, information and ideas, we make it possible. We are headquartered in St. Louis and have manufacturing capabilities in North America, Europe, Asia and Africa. For more information, visit us at www.belden.com; follow us on FacebookLinkedIn and X/Twitter.

BDC-Financial

For more information, contact:

Mary Melchiorre
Manager, Corporate Marketing Communications
+1-514-207-6106
[email protected]

 

Belden and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden and other parties may also have trademark rights in other terms used herein.