St. Louis, Missouri – July 9, 2026 – Belden Inc. (NYSE: BDC), a leading global provider of complete connection solutions, today announced the release of its new ProSoft Technology ELX3 ProLinx Edge™ Gateway. This offering unites operational technology (OT) protocol conversion with lightweight, Docker-based edge application hosting on a single ruggedized hardware platform—enabling organizations to deploy data acquisition, digital connectivity (including digital twin/asset monitoring) and CPU-based edge analytics directly at the machine level. The gateway gathers and processes data at the network edge for localized decision-making.
As digitization and industrial internet of things (IIoT) transformations push forward, organizations have new opportunities to extract, analyze and act on OT data to propel efficiencies, reduce scrap and waste and reach sustainability targets. The ProLinx Edge Gateway is designed for large, complex industrial networks with a growing number of connected devices. Manufacturers and energy operators in industries such as oil & gas, power distribution and warehousing and logistics can run compact AI inference models, digital twin connectivity agents and near-real-time analytics containers alongside proven EtherNet/IP™–to–Modbus TCP/IP protocol gateway functions—all within a single device rated for harsh environments.
The gateway offers powerful features that empower organizations to:
- Achieve OT protocol conversion by enabling EtherNet/IP™ and Modbus TCP/IP data exchange to allow for communication between dissimilar devices in the field.
- Deploy user-defined containers by empowering custom code and algorithm creation for advanced applications like machine learning and predictive maintenance, digital twin/asset monitoring and near-real-time analytics.
- Future-proof edge deployments with a platform designed to expand as additional protocol container gateways are released.
“The ELX3 is ideal for industrial companies looking to unite data from disparate IIoT devices and legacy OT equipment, bringing silos of automation into centralized systems for analysis and action.” said Erik Syme, Director of Program Management, ProSoft Technology. “By supporting both ProSoft protocol gateway containers and custom containers, the ELX3 gives users the flexibility they need to address today’s most demanding edge applications and scale as their operations evolve.”
Engineered to withstand shock, vibration and electromagnetic compatibility (EMC) tolerances, with a temperature range of -40ºC to +70ºC, and rated for Class I, Division 2 environments, the ProLinx Edge Gateway is suitable for use in harsh environments. An industrial-grade solution, the gateway addresses the complex requirements of varied industries, including automotive, consumer packaged goods, food and beverage, machine building, process manufacturing, warehousing and logistics, metals, mining, oil and gas and water and wastewater.
Learn more about the ProLinx Edge Gateway.
About Belden
Belden Inc. delivers complete connection solutions that unlock untold possibilities for our customers, their customers and the world. We advance ideas and technologies that enable a safer, smarter and more prosperous future. Throughout our 120+ year history we have evolved as a company, but our purpose remains – making connections. By connecting people, information and ideas, we make it possible. We are headquartered in St. Louis and have manufacturing capabilities in North America, Europe, Asia and Africa. For more information, visit us at www.belden.com; follow us on Facebook, LinkedIn and X/Twitter.
For more information, contact:
Scott Todd
Manager, Public Relations and Thought Leadership
[email protected]
Belden and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden and other parties may also have trademark rights in other terms used herein.